VBUS.CAP
Description
This parameter reports the DC bus capacitance for the drive. The capacitance value is determined by the drive model.
Examples
Usage
VBUS.CAP is used to calculate bus voltage ripple and detect phase loss at the AC line input to the DC bus. When phase loss is detected, the drive reported Fault "F2008": Bus capacitor overloaded.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
microfarads |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
VBUS.CAP |
300ah |
0bh |
Unsigned16 |
- |
- |
Read only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
2501 |
1 |
2501 (0x9c5) |
VBUS.CAP |
Unsigned32 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
VBUS.CAP |
2501 |
Unsigned32 |
Read Only |
- |